D3349890_04

Fan Switch

A Fan Switch widget switches fan On and Off.

To configure Fan Switch:

  1. In General tab, enter the Title of the widget.

  2. In Objects tab, select the Switch object for the Fan Switch from the drop-down.

    Fan Switch supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Switch

      • Start/Stop

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.