D3349890_04

Light Switch

The Light Switch widget enables you to turn On/Off the load and facilitates the creation of a singular switch for on/off control.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Light Switch.

  3. Tap on the widget’s label to operate the Light Switch. The Light Switch screen appears.

On State

Off State

Example: You can set the Light Switch to turn lights on and off in different rooms. You can set it up to control individual lights, making it easy to manage your home’s lighting with a single tap.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.