D3349890_04

Socket Switch

A Socket Switch widget allows you to switch on and off the loads.
  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Socket Switch.

  3. Tap on the widget's label to operate the Socket Switch.

    The Socket Switch screen appears.

On State

Off State

Example: You can use the Socket Switch widget to control holiday lights and decorations, making it easy to turn them on or off without having to unplug them.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.