D3349890_04

Air Conditioner Switch

Air Conditioner (AC) Switch widget switches AC On and Off.

The functions supported by the widget are:

To operate AC Switch:

  1. Click anywhere on the widget to turn On/Off the AC switch.

On State

Off State

Example: If AC Switch widget is configured, you can control the AC remotely. If your coming home earlier than expected, you can turn on the AC using the widget so the home is cool when you arrive.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.