D3349890_04

AC Switch

The AC Switch widget facilitates the switching of the AC On and Off, supporting the on/off function.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the AC Switch.

  3. Tap on the widget's label to operate the AC Switch.

    The AC Switch screen appears.

  4. Tap on the widget to turn the AC on or off.

On State

Off State

Example: If AC Switch widget is configured, you can control the AC remotely. If your coming home earlier than expected, you can use the widget to turn on the AC, ensuring a cool and comfortable home upon arrival.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.