D3349890_04

Lighting Preset

The Lighting Preset widget is used for setting a load to a preset level (from 0% to 100%).

The functions supported by the widget are:

Lighting Preset widget allows you to create either one or more labels (maximum 3).

NOTE: Only one preset level can be set at a time.

To operate the Lighting Preset :

  1. Click on the required label.

The selected label is set to its preset level.

NOTE: If any of the configured preset value is not currently set or active, the widget is displayed in an off state.

On State

Off State

Example: You can set Lighting Preset widget with different labels such as:

  • Work Mode: You can set a preset for your home office with bright, cool lighting to keep you alert and focused during work hours.

  • Relaxation: You can create a preset with soft, dim lighting for relaxation or meditation sessions which can help to unwind after a long day.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.