D3349890_04

Enable Preset

The Enable Preset widget enables the preset level and permits the creation of a single preset label.

NOTE: If any of the configured preset value is not currently set or active, the widget is displayed in an off state.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to enable the preset level.

  3. Tap on the widget's label. The Enable Preset screen appears.

  4. Tap on any of the configured preset value to set the preset level.

On State

Off State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.