D3349890_04

Enable Cloud Connector and IoT Third Party API

The home page of the Network Automation Controller is shown below:


  1. Open the Cloud connector, the Settings pop-up appears.

  2. Select the Enable Cloud Connector checkbox.

    The below table illustrates the icons used to represent the application status:

    Cloud Connector

    Connected

    Cloud Connector

    In the connection process

    Cloud Connector

    Not able to connect

    Cloud Connector

    Disabled

    NOTE: Cloud Connector will be connected only after pairing is done through Management app.
    NOTE: Please be aware that other services, such as homekit, voice control, and energy monitoring, have not yet been implemented for the C-Bus controller as of today (v2.1.0) and will not be available for use.
  3. Open the IoT Third Party API application, the Settings pop-up appears. Enable the API for Cloud connection, local network and third party application data.

    The below icon shows the status of the application:

    • Dark grey icons of the cloud or network – remote or local access to the IoT third party API is enabled.

    • Light grey icons of the cloud or network – remote or local access to the IoT third party API is disabled.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.