D3349890_04

Control Moments from Your Home Screen

To control moments directly from your Home screen, turn on the Show Moments feature.

  1. Tap > Home screen > enable Show Moments.

  2. All the moment tiles are now displayed on the Home screen. You can scroll through them and turn them on.

NOTE: Moments cannot be edited or deleted from the Home page.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.