D3349890_04

Fan Controller

The Fan Controller widget allows to control the speed of a fan.

Fan Controller widget allows you to create different modes and set speed name and speed value for each mode.

Initially, three modes - slow, medium, and fast are set up by default. These can be adjusted, and up to five modes can be configured.

  • Click on (<) or (>) buttons to change the fan modes.

  • To turn on, click anywhere on the widget.

  • To turn off, being on the fast mode click (>) button.

To configure Fan Controller:

  1. In General tab, enter the Title of the widget, and Number of speeds, Speed Name, and Level Value.

  2. In Objects tab, select the Value object for the Fan Controller from the drop-down.

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.