D3349890_04

Bellpress

The Bellpress widget is used for momentary activation of a load, for example a doorbell.

To configure Bellpress:

  1. In General tab, enter the Title of the widget.

  2. In Objects tab, select the Value Object 1 for the Bellpress from the drop-down.

    Bellpress supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Bellpress

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.