Manager
You can organize widgets by mapping them to your home's layout, specifying the floors, rooms, and exact locations for each one of them.
To access Manager from the home page of controller application,
click
.
Manager application consists of four main sections:
Home
The home page of the Manager is shown below:
You configure the greeting and weather information displayed on the home page in Manager Config settings.
To quickly access widgets, select the Show Widget on Main Page checkbox during configuration to add them as Favorites on the home page.
Home page displays all the favorite widgets.
To edit the widgets in the Manager application:
-
Unlock
ellipse icon on each widget to set the General and Schedulers settings.
Floor and Room
The floor section displays all the floors in your home created in the Manager Config application. The room section displays all the rooms created in the floor.
To navigate to floor and room :
Alarm Panel
The Alarm Panel widget allows you to monitor C-Bus enabled security panels.
- Enter the security code and click Enter to disarm the Alarm Panel widget.
NOTE: The Armed page appears only when a security code has been set and Alarm Panel widget is locked.
The quick functions window appears.
-
Click the Security drop-down to view the additional options.
-
You can either:
-
Click Zones from the drop-down list.
or
-
Click Zones from the widget section to open the Zones section.
You can view the zones that are configured in Manager Config.
Refer the below table for color and alert indicators:
-
-
Click Tap to see more in View Keypad widget to navigate to Alarm Panel main (Disarmed) page.
-
You can either:
-
Click Alarms from the drop-down list.
or
-
Click Alarms from the widget section to open the Alarms section.
You can view the alarms that are configured in Manager Config.
Refer the below table for color and alert indicators:
-
Functions
The functions section allows you to view and control the widgets based on the selected function type.
Below are the available function types:
-
Lighting
-
Climate
-
Blinds
-
General
-
Scenes