D3349890_04

Adding Device to Favorites

You can mark devices as favorites and access them directly from the Home screen in the Favorites section.

  1. On the Home screen, locate the device which you want to mark as a favorite.

  2. Tap the device. The control screen appears.

  3. Tap at the top right.

    The device appears under the Favorites section for the relevant floor and associated rooms.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.