D3349890_04

Lighting Status

The Lighting Status widget displays the current status of a specific light, allowing you to see whether the light is on, off, or in any other state.

To configure Lighting Status:

  1. In General tab, enter the Title of the widget.

  2. In Objects tab, select the Value Object for the Lighting Status from the drop-down.

    Lighting Status supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Switch

      • Up/Down

      • Open/Close

      • Boolean

      • Dimmer

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.