D3349890_04

Enable Preset

The Enable Preset widget is used to enable the preset level.

The appearance of the widget depends on the number of labels created for an object. At least one label must be created, with a maximum of three labels allowed.

NOTE: Only one preset level can be set at a time.

Enable Preset with 1 label

NOTE: If any of the configured preset value is not currently set or active, the widget is displayed in an off state.

To configure Enable Preset:

  1. In General tab, enter the Title of the widget, Preset Label and respective Preset Value (0–255).

  2. In Objects tab, select the Value Object for the Enable Preset from the drop-down.

    Enable Preset supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Switch

      • Up/Down

      • Open/Close

      • Boolean

      • Dimmer

      • Enable

      • Invert Enable

      • High/Low

      • Start/Stop

      • Boolean Boolean

      • Boolean Inversion

    • Enable Application

    • Trigger Application

    • User Parameter

      • Boolean

      • Signed

      • Unsigned

      • RGB

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.