D3349890_04

Weather Panel

You can enable the Weather Panel during the final step of the registration process or in the Settings. The weather panel displays the weather updates for the address entered in the Home Management section. (Home Management).

To view the weather information on your Home screen:

  1. Tap > Home Screen > Weather Panel > tap the Show Weather Panel toggle button.

  2. Select the required unit (°C or °F) from Temperature Units drop-down list.

  3. In WEATHER STATION section, tap the Use on-line weather service toggle button to enable the online weather service.

    Mouse over on the to view the tooltip.

  4. Tap to close the pop-up.

  5. Tap Save.

    NOTE:

    If the controller’s Consents (refer Consents) is turned off, and you attempt to turn on the Use on-line Weather Service toggle button, the Weather Legal Statement screen will appear. Tap Accept to proceed.

    TIP: Turn on the Controller Consents, Show Weather Panel , and Use on-line weather service toggle buttons to display weather information on your Home screen.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.