D3349890_04

Light Switch

The Light Switch widget is used for On/Off control of a load.

Below are the functions supported by the widget:

Light Switch widget allows you to create either individual switch or multiple switch (maximum 6).


Operations:

  • Individual switch: To control individual switch On/Off, click anywhere on the widget.

  • Multiple switches: To control multiple switches On/Off, click the large bulb icon.

  • To control individual switch among the multiple switches, click the small individual switch (small bulb icon).

NOTE: Individual switch can be named.

Multiple switch On State

Individual switch Off/On

Multiple switch Off State

Example: You can set the Light Switch to turn lights On and Off in different rooms. You can set it up to control individual lights or groups of lights, making it easy to manage your home’s lighting with a single tap.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.