D3349890_04

Clipsal C-Bus Manager Mobile App

Requirements for C-Bus System

To use the Clipsal C-Bus manager mobile app, follow the below prerequisites:

C-Bus controller

(5500AC2 and 5500NAC2)

  • Hardware version 1.1

  • Firmware version – 2.0.0 or higher

The C-Bus controller handles the visualization of the C-Bus devices and loads associated in the installation and enables communication with the Clipsal C-Bus manager mobile app.

C-Bus project and a running installation

All C-Bus devices installed and configured

This has to be done by a qualified system integrator or an electrician.

Internet access for the controller

To use the Clipsal C-Bus manager mobile app, it is essential for the C-Bus controller to be connected to the Internet through a router.

 

Supported devices

For more information, read Widget Based Visualization.

 

Smart phone

  • iOS version 13.4 and higher

  • Android version 10 and higher

 

Clipsal C-Bus manager mobile app

For more information, read Installing the Clipsal C-Bus Manager Mobile Application.

 

A valid e-mail address

To set up the Clipsal C-Bus manager mobile app, register an account with Schneider Electric with a valid e-mail address.

 
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.