D3349890_04

General Switch

General Switch widget is used to On/Off the individual loads.

The functions supported by the widget are:

To operate General Switch:

  1. Click anywhere on the widget, to On/Off the General Switch.

On State

Off State

Example: You can use the General Switch widget to turn lamps or overhead lights On and Off remotely.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.