D3349890_04

Rooms

Each floor accommodates multiple rooms.

You can:

  • Add a room

  • Edit the room name

  • Copy a room

  • Delete a room

Add a Room

To add a room:


Pre-requisite: Floors should have been created.

  1. Select the floor level, in which you want to create a room.

  2. Click ADD NEW ROOM to create a new room.

  3. Enter the room name in the text prompt and press Enter. The room page is created.

  4. Once the room is added, click ICON to create an icon for the room.

    Icon window is displayed as shown below.

  5. Select the respective icon for the room. Icon is added to the selected room.

Edit the Room name

To edit the room name:


Pre-requisite: Floors and rooms should have been created.

  1. In the room page, hover the cursor on the room name and click next to the room name.

  2. Enter the new room name and press Enter.

Copy a Room

To copy room details from one floor to another:


Pre-requisite: Floors and rooms should have been created.

  1. Navigate to the specific room page, click (visible at the top-center of the room page).

    Copy room window is displayed.

  2. Select the floor to which you want to copy the current room details and click Copy. The room details (widget and name) are copied to the selected floor.

Delete a Room

To delete a room:


Pre-requisite: Floors and rooms should have been created.

  1. Navigate to the specific room page, hover the cursor on the room name and click x to delete the room.

    A confirmation message is displayed.

  2. Click OK. The room is deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.