D3349890_04

Create Your User Account

If you are a new user, create an account for the Clipsal C-Bus manager mobile app.

  1. On the welcome screen, tap Get started.

  2. On the login screen, tap Register to create an account.

  3. Fill in the Registration form.

  4. Read the Privacy notice and then accept the Terms of use.

  5. Tap Continue.

    NOTE: An e-mail with a verification link will be sent to your e-mail address. Click the link and verify your account. (The link expires in 24 hours)
  6. Return to the application and log in (Logging In).

  7. After your first login, click Accept to grant the following access privileges:

    1. Clipsal C-Bus Cloud integration with OneSignal Service.

    2. By signing in, you are authorizing Clipsal C-Bus Cloud to access your C-Bus devices and scenes.

      NOTE: The password must meet at least the following criteria:
      • Eight characters long.

      • Contain at least one uppercase letter.

      • Contain at least one number.

      • Contain at least one special character.

        TIP: Increase the security of your password by observing the following points:

      • Do not use any personal information such as a name, birthday, email address, etc. These data are publicly visible and make it easier to guess the password.

      • Use a long password. It should contain at least eight characters; longer passwords help increase security.

      • Do not use a password that you have already assigned for another service.

      • If possible, include numbers, special characters and differences in upper and lower case.

      • Change the password frequently.

        TIP: For more information about hardening your network, refer Hardening Your System.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.