D3349890_04

Socket Switch

A Socket Switch widget is used to switch On/Off the individual loads.

The functions supported by the widget are:

To operate the Socket Switch:

  1. Click anywhere on the widget to On/Off the Socket Switch.

On State

Off State

Example: You can use the Socket Switch widget to control holiday lights and decorations, making it easy to turn them On or Off without having to unplug them.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.