D3349890_04

Add Moments

To add moments:

  1. On the Home screen (Home Screen), tap > tap at the bottom right of the Moments tab. The Moment creator page appears.

  2. Enter the name of the Moment and assign it an icon.

  3. Tap Add Actions. Select devices screen appears.

  4. Select the list of devices and tap Done.

  5. Tap on each device in your action list and set its behavior (for example, plugs on, lights off) on the control screen.

  6. Tap Set at the upper right corner of the device control screen.

    Repeat for all devices.

  7. After setting all the conditions, tap Save in the Moment creator.

    Once the Moment is saved, it will appear on the Moments tab. Tap on the Moment to enable it.


You can add any device in your home. For your convenience, you can also filter the devices by room.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.