D3349890_04

Fan Switch

Fan Switch widget is used to switch fan on and off.
  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Fan Switch.

  3. Tap the widget's label. The Fan Switch screen appears.

  4. Tap to turn the device on or off.

On State

Off State

Example: You can use the Fan Switch widget to turn off the fan when you leave the house and turn it back on just before you return. This way, you can save energy and still come back to a cool home.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.