D3349890_04

Notifications

Notification is a message or alert that appears on your mobile device to inform you about updates, reminders, or new information related to the app.


To access the Notifications:

  1. Tap > Notifications.

  2. Tap Enable Notifications toggle button to turn On/Off the notifications.

NOTE: Enabling/disabling notifications is related to your phone, not the Controller. The notification settings of one user account does not affect the other user account notification settings. Also, only system notifications will be triggered, other alerts are not supported.
NOTE: If you disable the notifications, you will not receive any notifications from the Controller or Schneider notifications (e.g. cloud outage).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.