D3349890_04

Two-State Enable

Two-State Enable widget is used to set the state of a load and it also supports on/off, enable/disable functions.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Two-State Enable function.

  3. Tap Start or Stop on the widget to turn on/off.

On State

Off State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.