D3349890_04

Bellpress

The Bellpress widget is used for the momentary activation of a load, such as a doorbell.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the Bellpress function.

  3. Tap PRESS to activate the Bellpress function.

Off State

On State

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.