D3349890_04

Manager Config

The Manager Config application enables you to create a visual layout of floors with multiple rooms.

To access the Manager Config from the Home page:

  1. Click Manager Config . The Home page of Manager Config is displayed.

Settings

To access the settings page:

  1. In the Home page, click to modify Manager Config settings.

    The following options are available.

    • Backup config : Enables you to save the current configuration details of a Manager Config application in JSON format.

    • Restore backup : Enables you to recover the preserved configuration details (in JSON format) of the Manager Config application.

    • Settings : Enables you to modify general setting of the Manager.

    • Styles : Enables you to modify appearance of the Manager Config application and widgets.

    • Clear All : Enables you to clear all the settings of rooms, widgets, and styles.

Settings

The Settings manager enables you to configure the Home Page and Weather for Manager/Manager Config home page.

  1. Click and select Settings from the list of options.

    Settings manager window is displayed.

  2. In the Screensaver timeout field, enter the seconds.

  3. In Home Page setting, enter the text in Welcome Text fields.

    NOTE: In the event of a change in the Controller system time, this greeting is automatically adjusted to reflect the appropriate time of day.

    TIP: You may configure a greeting and your family name in the Welcome Text field to appear in the Home page.

  4. In the Weather Setting, provide the required details.

    NOTE: Min or Current temperature, Max temperature (forecast) and Weather condition (Levels) are obtained from the user parameter objects.

    To set the real time weather, refer Weather Configuration.

  5. Click Save to save the configured settings.

The Home Page and Weather settings are displayed in the Manager/Manager Config Home page as configured.


Manager Config home page

Manager home page

Styles Manager

Styles manager allows you to customize the appearance of the Manager Config application and widgets. The configured style is reflected in Manager/Manager Config.

  1. Click and select Styles from the list of options.

    Styles manager window is displayed.

  2. Select the predefined themes from the Preset themes drop-down.

  3. Select the Hide lock button checkbox to hide the lock button.

  4. Select the Hide close button checkbox to hide the close button.

  5. Select the color code from the Background drop-down to change the background color of the Manager/Manager Config.

  6. Select the Preset Background to change the preset background of the Manager/Manager Config.

  7. Click to download the full project data in JSON format.

  8. Click to directly upload the project data in JSON format.

  9. Click Save to save the style settings.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.