D3349890_04

Shutter Relay Vertical

Shutter Relay Vertical widget is used to operate electric curtains, blinds, and shutters.

The functions supported by the widget are:

It has dual-control functionality which enables to handle both blinds and shades together. Shutter and blinds can be controlled individually using slider.


To operate the Shutter Relay Vertical :

  1. Click ˅ and ˄ buttons to open/close the shutter and blinds.

  2. To control the blockout and shade together, use the dual control.

Dual state off

Dual state on

Shutters and blinds controlled individually using slider

You have shutters installed in your home and you have set up a Shutter Relay widget in your smart home system. Using this widget, you can conveniently open or close the shutters with a simple tap on the widget.

If you want to let in natural light in the morning, you can use the widget to open the shutters.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.