D3349890_04

Info 2

Info 2 widget displays the values of the object assigned.

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to view the information.

Example: You can use the Info 2 widget to display the error messages and status from the various devices configured.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.