D3349890_04

Change Over Relay

The Change Over Relay actively manages blinds, curtains, or shutters with motors that require changing polarity. It directs two control group, one for opening and another for closing ensuring that only one group operates at a time. Shutter Relay is used for controlling blinds, curtains, or shutters with a single control group. It is suitable for setups where blind positioning is required.

To configure Change Over Relay:

  1. In General tab, enter the Title of the widget.

  2. In Objects tab, select the Up/Open Object, and Down/Close Object for the Change Over Relay from the respective drop-down.

    Change Over Relay supports the following type of objects:

    • Lighting applications

      • Legacy Lighting

      • Up/Down

      • Open/Close

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

    NOTE: Open, Pause and Close functions are configured by default.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.