D3349890_04

Floors

Manager Config allows you to create multiple floors.

You can:

  • Add a Floor

  • Edit the Floor Name

  • Switch between Floors

  • Delete a Floor

Add a Floor

To add a floor:

  1. Click ADD NEW FLOOR to create a new floor.

    A text prompt is displayed.

  2. Enter the floor name in the text prompt and press Enter. The floor page is created.

    TIP: Drag and drop the floor level in the suitable grid position to rearrange the floor’s position.

Edit the Floor Name

To edit the floor name:

  1. In the floor page, hover the cursor on the floor name and click .

  2. Enter the new floor name and press Enter.

    The new floor name is displayed.

    NOTE: When you rename a floor in the Manager Config, it will immediately reflect in Manager and take upto 2 minutes for the change to reflect in the mobile app.

Switch Floors

To switch between floors:

  1. Click any floor name. Floor page is displayed.

  2. Click the drop-down menu to select an alternative floor to switch from the current floor.

Delete a Floor

To delete a floor:

  1. Hover the cursor on the floor name and click x to delete the floor.

    A confirmation message is displayed.

  2. Click OK. The floor is deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.