D3349890_04

General Lighting Dimmer

The General Lighting Dimmer widget allows the you to control the level of a load from 0% to 100%. You can tap on the widget to turn the dimmer on or off, and use the level slider to increase or decrease the brightness. The General Lighting Dimmer widget is used for level control of a load (from 0% to 100%).

  1. Once you log in, the Home screen appears.

  2. Tap the room in which you want to control the General Lighting Dimmer .

  3. Tap on the widget's label to operate the General Lighting Dimmer.

    The General Lighting Dimmer screen appears.

On State

Off State

Example: You can use the General Lighting Dimmer widget to create a night light effect, offering just the right amount of illumination for comfort without being overly bright.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.