D3349890_04

Mounting the Controller

  • Install the C-Bus controller in the low voltage electrical cabinet.

    It is powered by a 24 V power supply and connected to the C-Bus network through C-Bus cables or IP.

  • Connect the C-Bus controller to the Internet router.

    Without Internet, the C-Bus controller cannot be controlled via the Clipsal C-Bus manager mobile app.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.