D3349890_04

Widget Based Visualization

The system integrator installs and configures the C-Bus project, creates a widget based visualization with the C-Bus devices in Manager application.

Manager visualization is then converted to the visualization in the Clipsal C-Bus manager mobile app (as explained in Creating Manager Visualization).

In Manager visualization, you can add your devices and change their parameters. You can add other elements at any time later.

NOTE: Only the widgets configured in Manager/Manager Config will be displayed in mobile app.
Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.