D3349890_04

Light Switch

The Light Switch widget is used for On/Off control of an individual load and multiple loads.

The appearance of the widget depends on the number of objects selected.

To configure Light Switch:

  1. In General tab, enter the Title of the widget, and the respective lights title.

    • You can assign titles for multiple loads by entering a name for each widget in the designated fields. For example, enter Light 1 title for the first widget, Light 2 title for the second widget, and Light 3 title for the third widget.

    • If you don't assign names for the multiple loads, the default field name is taken as widget’s name.

  2. In Objects tab, select the lighting objects for the Light Switch from the drop-down.

    • Light Switch supports the following type of objects:

      • Lighting applications

        • Legacy Lighting

        • Switch

        • Up/Down

        • Open/Close

        • Boolean

        • Dimmer

    • If only one switch object is selected, the widget looks as shown below.

    • If more than one switch object is selected, the widget looks as shown below.

      All the switches can be controlled in a load and each switch can have names.

      • Click on Tap to turn off or big bulb icon to control all switch on/off in group.

      • To switch individual lighting circuits/objects on/off, click on individual small bulb icons.

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.