D3349890_04

Installing Manager/Config Application into 5500NAC2

The Manager/Config application comes pre-installed on the 5500AC2 after upgrading to v2.0.0 and above. However, for the 5500NAC2, the Manager/Config application is not pre-installed, but you can install it manually.


Below are the steps explained on how to install the Manager/Config on the 5500NAC2.

  1. On home page, click to open configure apps page.

  2. In the configure apps page, click on to install the Manager application into 5500NAC2.

  3. Once installed, the Manager/Config application is available in 5500NAC2 as shown below.

The operations and functions outlined for the 5500AC2 are equally applicable to the 5500NAC2.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.