D3349890_04

Widgets

Widgets represent functions or automations that can be managed or monitored via the Manager application.

The following widgets can be added to each room.

  • Light Switch

  • Fan Controller

  • General Lighting Timer (Not supported in Mobile App)

  • Bellpress

  • Enable Preset

  • Socket Switch

  • AC Switch

  • Shutter Relay Horizontal

  • Shutter Relay Vertical

  • Fan Switch

  • General Switch

  • Change Over Relay

  • Lighting Preset

  • Lighting Status

  • Local Scene Controller

  • Two-State Enable

  • Info 1

  • Info 2

  • General Lighting Dimmer

  • Scene Trigger

You can add a widget, edit the widget name, copy a widget and delete a widget

NOTE: Each configured widget can be imported or exported to another controller.

Add a Widget

To add a widget in a room page:

  1. Select the respective floor and navigate to the room to add widgets.

  2. Click + (visible at the top right corner).

    The Add New Widget menu slides out from the right side which displays all the available widgets.

  3. Click on the required widget to add to the room.

    Settings window is displayed.

    Example:

  4. In the General tab, enter the name for the widget in the Title field and click Save.

    • You can assign titles for multiple loads by entering a name for each widget in the designated fields. For example, enter Light 1 title for the first widget, Light 2 title for the second widget, and Light 3 title for the third widget.

    • If you don't assign names for the multiple loads, the default field name is taken as widget’s name.

  5. Click Objects tab and select the objects you want to control from the drop-down.

    NOTE: These objects are from the object list created in the configurator.
  6. Click Styles tab and select the Show Widget on Main page check box to add widget as favorite on the home page.

  7. Click Save to save the widget.

    Widget is displayed in the room page and also on the main page in favorites.

Edit the Widget Name

To edit the widget name:

  1. Hover the cursor on the top right of a widget and click .

    Settings window is displayed.

  2. Make necessary changes and click Save.

  3. Drag and drop the widget in the suitable grid position to rearrange the widget’s position.

Copy a Widget

To copy the widget details:


  1. Hover the cursor on the top right of the widget and click to copy a widget from one room to another. Copy widget window is displayed.

  2. Choose the room to which you want to copy the current widget and click Copy.

Delete a Widget

To delete a widget:


  1. Hover the cursor on the top right of the widget and click x to delete the widget. A confirmation message is displayed.

  2. Click OK. The widget is deleted.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.