View Existing Geodatabase Regions

Existing Geodatabase Regions are listed along the left-hand side. Your total count of Geodatabase Regions is displayed at the bottom of the list.

Use the drop-down to sort the list of Geodatabase Regions.

NOTE: Use the Search field along the top of Solution Center to search through the list of existing Geodatabase Regions.

Click any existing Geodatabase Region to view more information, including:

  1. Utility Domain.

  2. Storage GlobalID. If needed, you can click the Copy to Clipboard icon to paste this information into another application, email, etc. You can also download the Geodatabase Region Resource (GRR) file by clicking the Download File icon, after which the Show in Folder icon appears—clicking it opens the folder to which the GRR file is downloaded.

  3. Feeder ID. If needed, you can click the Copy to Clipboard icon to paste this information into another application, email, etc.

  4. Last Requested. This is the date and time the application most recently requested an update from the geodatabase.

  5. Last Updated. This is the date and time the feeder or region was most recently updated with any changes from the geodatabase. Under normal circumstances, it is a few minutes after the “Last Requested” date and time (the difference between the two timestamps is the amount of time it took to process the updates). If there was an error during the update, the application alerts you via a notification and labels the feeder or region with an error icon so that you may investigate and remedy the error.

  6. Availability Status. These include:

    1. Available: The feeder or region is ready for use by designers in the Designer XI client application.

    2. Pending: The feeder or region is currently undergoing an update to reflect any changes from the geodatabase. In normal circumstances, it changes to “Available” in a few minutes.

    3. Error: Something happened during the create or update process that is preventing the use of the feeder or region. See the Error Remediation topic for tips on resolving the error.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.