Session Manager

If using the Hosted Edge along with Esri’s geometric network and Process Framework Session Manager, the database connection strings must be populated in Solution Center > Designer > Mapping > Session Manager.

  • This is the same configuration with the same settings as on-premises Edge Service.

  • The key difference is that the configuration is performed in Solution Center > Designer > Mapping > Session Manager instead of the app.config file.

IMPORTANT: This requires the feature flag Designer/SolutionCenter/SessionManagerConfig.

Along the left-hand side there are three options:

  • Default: You can configure database connection strings to satisfy both Electric and Gas. In other words, both types of designs use the same connection strings.

  • Electric: You can override the default and provide electric-only connection strings.

  • Gas: You can override the default and provide gas-only connection strings.

If you leave Electric or Gas empty, they “fall back” to the default.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.