Schedule Updates for Geodatabase Regions

Geodatabase Regions are snapshots of the feeder or region as stored in the geodatabase. They should be updated routinely so that the designers working in the Designer XI application have the most accurate information at their fingertips.

IMPORTANT:
  • You can update feeders or regions individually.

  • You can use the Ctrl and Shift keys to select multiple feeders or regions and then update them.

  • You can update all feeders or regions at any time by clicking the Update All button.

  • Given the processing time, the best practice is to schedule routine updates during off hours.

Existing schedules are listed along the left-hand side. Click an existing schedule to view upcoming days/time for the update.

To create a new schedule, follow these steps:

  1. Use the drop-down to choose Schedule.

  2. Click the Add New button.

  3. Type a Title for the schedule. We recommend a concise but descriptive title so that it is understandable at a glance. For example, “Sunday Night at 1:00 a.m.,” or “Every Night at 1:00 a.m.”

  4. For standard schedules, use the Weekly Scheduler. This allows you to choose days and set the same start time for all chosen days. In the following image, the update starts at 1:00 a.m. on Sunday and Wednesday.

    1. Choose the Start Time.

    2. Choose the Days.

      IMPORTANT: Do you see an option to “Only Update GRRs with Deltas?” This handy option is for electric customers on the Utility Network (UN) and those who have implemented Geodatabase Manager XI. Other applications, such as Feeder Services, already support the electric UN fully, which is why the toggle is present. For more information, see the description for the UpdateLastUpdateSubnetworkTimeStamps Action Handler in the Action Handlers topic of the Geodatabase Manager XI Configuration Guide.

    3. Click Save.

    NOTE: You can have multiple schedules to accommodate different start times. For example, you can have an update for Wednesday start at 1:00 a.m., and have a separate schedule for Sunday to start at 3:00 a.m.

  5. For advanced schedules, use the Custom Scheduler. This allows you to create a crontab expression to accommodate situations like “First of the Month,” or “Every Third Week,” etc.

    1. The dialog provides template examples. Click an example to see the equivalent crontab expression.

    2. Hover over the expression to see a tool tip that labels the parts of the expression.

    3. Search “crontab expression” on the web to see more examples or find an expression builder to assist you.

  6. After populating the expression, click Save.

NOTE: If something occurred during a scheduled update that prevented the update from completing, you can click the existing schedule and then click Restart. However, be aware of the processing time required. Processing time varies by company and size of feeders and regions. Over time, you get a feel for how long schedules take to complete.


Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.