Equipment

The Equipment tab allows you to create and edit the attributes that inform the specifications of the electrical component.

Use the Jump To shortcut to switch to a Related CU. This brings you to the selected object. Click on the Equipment tab to return. For more information about the relationship between CUs and Equipment Specifications, see the topic Relate a CU to an Equipment Specification.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.