Advanced Tab

The Advanced tab contains other technical configurations. The available functions vary with the stage of your implementation. Some of these configurations are used during implementation and then turned off at project initialization.

Other functions, like Workflow Buttons and Dynamic Workflow Buttons, are legacy options to create buttons for custom workflows. While these options appear in some tenant instances, Designer Client Workflows showcases the best practice for creating client-side workflows specific to the Designer XI application.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.