Work Areas

Work Areas are the “footprint” or boundary of the design. They are particularly helpful to give designs a defined space, and to inform other designers of activity in the area. The symbology (fill, style, and outline) are configurable at the company level, and the following image is just an example.


Prerequisite: The Work Area Must be in the Published Map Service

Before you can configure the Work Area in the Work Areas tab, the feature class itself must be included in the published map service. This is the map service found on either the Electric Options or Gas Options subtab.

  • If your company is utilizing the GIS Push Feature Service, then the Work Areas subtab consumes this published service.

  • If your company is not utilizing the GIS Push Feature Service, then the Work Areas subtab consumes the Network Feature Service.

When creating the Work Area feature class, follow these guidelines:

  • It must be a polygon.

  • It must be included in the published map service that satisfies the Network Feature Service. Do not worry about its symbology in the feature service, as you set the symbology in the Work Areas subtab.

  • Because it is included in the Network Feature Service and because the other feature classes in that service are registered as versioned, the Work Area feature class must also be registered as versioned.

  • It must have the Required fields below.

  • You can change the field names below. However, later you map these fields in Solution Center, and if you name them as displayed in the table, it is easier to know which fields should be mapped together because the names are the same. Finally, you can increase the field lengths if your company attributes require more characters.

    Required/ Recommended

    Field Name

    Field Type and Length

    Description

    Required

    DesignID

    GUID

    Stores the Design ID created by the application

    Required

    WorkOrderID

    Text, 50

    Stores the Work Order ID generated by the integrated WMS

    Required

    Designer

    Text, 50

    Stores the name of the designer assigned to the job

    Required

    JobStatus

    Text, 50

    Stores the progress status of the design

    Required

    ObjectID

    Object ID

    Required field for all Esri feature classes

    Required

    GlobalID

    Global ID

    Auto-generated ID

    Recommended

    WorkflowStatus

    Short Integer

    Reserved for future use to track status independent of Job Status

    Recommended

    Description

    Text, 255

    Reserved for future use to provide a text field for designer notes


Map the Work Area to the Published Map Service

After successfully publishing the map service to include the Work Area feature class, you are ready to configure the Work Area in the application.

  1. In Mapping > Work Areas, click either Electric or Gas.

  2. Click Create.

  3. For Work Area Layer, use the drop-down to choose the Work Area polygon feature class included in the published map service. The name might differ from the image below, as it depends on what you named it in the service.

  4. Map the remaining fields to the appropriate fields in the Work Area feature class. The Names might vary from the image below depending on how you named the fields when you created the feature class.

  5. Click Save.


Choose Work Area Symbology

After mapping the Work Area fields, set the symbology of how the Work Area should look and feel in the map. You can have one symbology for electric and another for gas. When configuring the symbology, the best way to see how it is going to look is to set it in Solution Center, then open a design in Designer XI. When you re-open a design, the Work Area takes on the new symbology.

  1. Type a buffer width.

    1. As an example, a buffer width of 5 meters looks like this:

    2. And, a buffer width of 15 meters looks like this:

  2. Choose a Fill Style and Fill Color. The best way to view the symbology is in the Designer XI application, but here are examples of the Fill Style to get you going:

    Fill Style

    Symbology

    Backward Diagonal

    Cross

    Diagonal Cross

    Forward Diagonal

    Horizontal

    (None)

    Solid

    Vertical

  3. Choose an Outline Style, Outline Color, and Outline Width.

  4. Click Save.

  5. View a design in Designer XI to confirm the Work Area symbology.


Publish Operational Map for Work Areas

It is strongly recommended to include the Work Area polygon feature class either as its own standalone Operational Map or as a part of a larger Reference Map. In the former situation, you then create a Reference View from the Operational Map that only includes the Work Area. This is important because it allows designers to turn on the Work Areas in the Designer XI application to see what other work is happening in proximity to their design. Designers can, by default, see the Work Area for their current design, but it is through either a Reference Map or View that designers see other Work Areas.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.