CU Categories

Your company’s catalog of Compatible Units (CUs) is large and comprehensive. While end users can search for a CU using Name, Description, and WMS Code, you can help end users even more by configuring CU Categories. CU Categories allow end users to filter down the list of CUs while searching in the application. The following image is just an example, and you can configure any CU Categories you want.

Further, by establishing CU Categories, you enhance data integrity because the Category can guide a user to pick an appropriate CU given the design’s circumstances. For example, if the design is in an environmentally sensitive area, the designer could ensure the CUs they select are acceptable within that CU Category.

Configuring CU Categories takes place entirely within Solution Center. In short, you:

  1. Create CU Categories.

    • Name the CU Category.

    • Choose a color to help end users differentiate the categories.

    • Provide the acceptable values for each category.

  2. Create Non-Drawn CU Types.

    • If you do not plan on offering CU Categories for Non-Drawn CU Types, then this step can be ignored for the purposes of CU Categories. You can configure your Non-Drawn CU Types at any time and separately from CU Categories.

    • If you do plan on having CU Categories for Non-Drawn CUs, then the Non-Drawn CU Types need to be established before creating the CU Category Groups. Thus, this step must come before #3, Create CU Category Groups.

  3. Create CU Category Groups.

    • Assign the CU Categories to the appropriate component types.

  4. Assign CU Categories to CUs, Non-Drawn CUs, and Macro CUs (this can be accomplished in bulk using the Export/Import tools).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.