Compatible Unit

This tab provides information about the CUs in your system and helps you maintain their attributes.

For UN implementations, the combination of Layer Name plus the Asset Group and Asset Type defines an Asset Key. This key becomes important when determining where attributes came from and how they will be pushed in the GIS.

NOTE: CUs and Macro CUs must have a complete Asset Key in order to appear in CU search and be placed and interacted with in the design.

For GN environments, there are two options. You can configure a Subtype Key or use Layer and Subtype Rules.

Configuration of Subtype Keys for each CU is required for new GN implementations to enable Related Records functionality. A Subtype Key, or GUID, is assigned to each unique Layer plus Subtype code and is used in place of Layer and Subtype Rules. A Subtype Key is a unique identifier for a combination of a Layer and Subtype Code in the GIS. Defining the Subtype Key enables the filtered drop-down values when configuring GIS Attributes.

Existing GN implementations will have the choice to remain with legacy Layer and Subtype Rules or move to Subtype Keys. Notice in the image below that no Subtype Key has been defined since Layer Name and Subtype are blank. The Designer XI application would need to pull attribute information from the GIS, relying on Layer and Subtype Rules. This configuration is still supported, but we strongly recommend migrating to Subtype Keys to take advantage of new functionality.


On the Compatible Unit tab you can perform the following actions:

  • Click the Add button to add a new CU or add CU Attributes to an existing CU.

  • Click the Edit button to edit the Related Equipment Specification, change the Available Work Functions, or edit the assigned CU Categories..

  • Click Copy CU as a first step toward modifying and creating a new CU.

  • Click Delete to delete a CU.

  • Jump to an associated Related Equipment or Macro CU. This brings you to the selected object. Click on the Compatible Unit tab to return.

IMPORTANT: After making changes, always update the Catalog Cache.

For more information about the relationship between CUs and Equipment Specifications, see the topic Relate a CU to an Equipment Specification.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.