Re-Order the List of Design Styles

The order of Design Styles that you see in Solution Center is the same order end users see in the application. To re-order the list, follow these steps:

  1. In Solution Center > Designer > Client Application > Design Styles, find the list of Design Styles along the left-hand side of the dialog.

  2. Click and hold a Design Style name, then drag and drop it into a desired position.

  3. When you release the cursor, the new position is automatically applied. Users see the new order the next time they launch the application.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.