Configure Work Locations to Push to the GIS

By default, the Work Locations included in designs are not pushed back to the GIS along with the design components. If that is your company’s desired behavior, there is nothing for you to do.

However, if you want to push the Work Locations to the GIS along with the design, complete the steps in the subsequent sub-topics of this help chapter.


Create Work Location Feature Class

If you would like to push Work Locations from the design to your GIS, then you need a Work Location feature class ready to receive them.

IMPORTANT: You might already have a Work Location feature class, so verify before creating a new one.


Work Location Feature Class Minimum Requirements

When creating the Work Location feature class, follow these guidelines:

  • It must be a point.

  • The name of the feature class is up to you, but Schneider Electric recommends naming it Work Location.

  • It must be included in the published Network Feature Service. Ensure you re-publish the map service after creating the Work Location feature class.

  • For fields, follow these requirements and recommendations. In terms of the “Recommended” fields, they are all optional. It really depends what you want to track for your Work Locations.

    NOTE: As explained in the topic Add Work Location Name to Component Tables (Optional), you can also track Work Location attributes within the design components’ attributes. In other words, in addition to tracking information within the Work Location feature class, every design component could also store its Work Location information within its own attribute table.

    Required/Recommended

    Field Name

    Type

    Required

    GlobalID

    Global ID

    Required

    ObjectID

    Object ID

    Recommended

    DesignID

    GUID

    Recommended

    DesignName

    Text

    Recommended

    Name

    Text

    Recommended

    Number

    Integer

    Recommended

    ShortName

    Text

    Recommended

    WorkRequestID

    GUID

    Recommended

    WorkRequestName

    Text

    Recommended

    WorkRequestStatus

    Text


Map the Work Location Fields in the Schema

After creating the Work Location feature class and re-publishing the Network Feature Service, it is now time to inform the Schema of the Work Locations. To do so, follow these steps:

  1. In Solution Center > Designer > Catalog, click with the Electric GIS Schema or the Gas GIS Schema.

  2. Ensure the Schema drop-down is set to Tables.

  3. Click the Add Table button.

  4. For Designer Component, choose WorkLocation.

  5. For Layer, choose Work Location (this is the name of the feature class, so if you named it differently, locate your name appropriately).

  6. Under Fields, click the Add Field button. Here is where you decide which fields you want to capture within the Work Location feature class upon pushing the design to the GIS. The following image is just an example, and your desired fields can differ.

    • Check “Push to GIS” for each field.

    • Uncheck “Import” for each field. Importing Work Locations is not currently supported.

  7. Click Save.

  8. Restart the Edge Service to see the changes reflected in the Designer XI  application if you are using an on-premises version of the service. The Hosted Edge Service will pick up configuration changes as they occur. 


Add Work Location Name to Component Tables (Optional)

In addition to pushing the Work Location itself, you can also choose to store the Work Location Name within the components’ tables. For example, if you push a structure back to the GIS, the structure’s attribute table can include its Work Location Name.

  • Every Work Location has two names: Work Location Name and Work Location Short Name.

  • You can choose one name to push back to the GIS, but you cannot push both.


To map the Work Location Name or Short Name to the components’ tables, follow these steps:

  1. In Solution Center > Designer > Catalog, click Electric GIS Schema or Gas GIS Schema.

  2. Ensure the Schema drop-down is set to Tables.

  3. Click the component you want to configure.

  4. Under Fields, click the Add Field button.

  5. Map either the WorkLocationName or WorkLocationShortName to an appropriate GIS field such as WorkLocationID.

    • Check “Push to GIS” for the name field.

    • Uncheck “Import” for the name field. Importing Work Location fields is not currently supported.

  6. Click Save.

  7. Repeat for other desired components.

  8. Restart the Edge Service to see the changes reflected in the Designer XI application.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.