Configure Stamp Graphics

Stamp Graphics provide designers the ability to add graphics, details, and explanatory notes to their designs.

ArcGIS Pro is used to create and configure Stamp Graphics. The collection of graphics is saved as a .stylx file that is uploaded in Solution Center. See the Designer plugin topic Stamp Graphics for more information and steps to create or extend a Stamp Graphics Style.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.