D3349890_04

Zone Control

The Zone Control widget allows you to monitor and control the individual zones within the HVAC system.

You can configure objects for parameters such as Plant On/Off, Zone Open & Close, Zone Air Flow, Current Temperature, Zone Humidity, and Setpoint. You can monitor and control the zone from the Manager interface based on the mappings defined in Configurator.


To configure Zone Control:

  1. In General tab, enter the Title of the widget.

    NOTE: Once you select the objects in the Objects tab, based on the configuration defined in the Configurator, the corresponding values will be displayed in the Setpoint step, Temperature Unit, Setpoint minimum value, and Setpoint maximum value fields.
  2. In the Objects tab, select the Plant On/Off, Current temperature, Zone Humidity, Set Point, Zone Open & Close and Zone Air Flow objects from the drop-down list.

    NOTE: Only the objects that are created and configured will appear in the drop-down list for selection.

    Refer the below table for field description:

    Field

    Description

    Plant On/Off*

    Select the C-Bus object that represents the HVAC plant ON/OFF status. This value is displayed as read-only in the Zone Control widget and reflects the current state of the plant. You can also reuse the same object used for AC plant ON/OFF.

    Zone Open & Close*

    Select the C-Bus object that defines the status of the Zone.

    Zone Airflow

    Select the C-Bus object to control the airflow of the Zone.

    Current temperature

    Select the C-Bus object that provides the current temperature reading.

    Zone Humidity

    Select the C-Bus object that provides the current humidity level.

    Set Point

    Select the C-Bus object to define the desired temperature setpoint for the Zone.

    TIP: Fields marked with an asterisk (*) are mandatory.

    Refer to the table below for supported object type mappings.

    Object Field

    Supported Object Types

    Plant On/Off

    All Lighting objects without a specific function (legacy objects), Boolean, and User parameter (Boolean).

    Zone open/close

    All Lighting objects without a specific function (legacy objects, Switch, Open/Close), Boolean and User Param (Boolean).

    Zone Airflow

    All Lighting objects without a specific function (legacy objects).

    Current Temperature

    Measurement application, Unit parameter, and User parameter (Float/Integer).

    Current Humidity

    Measurement application, and User parameter (Float/Integer).

    Setpoint Temperature

    All Lighting objects without a specific function (legacy objects), Measurement application and User parameter (Float/Integer).

    Once you select objects in the Objects tab, the values in General section will be displayed.

  3. In Styles tab, select the Show widget on Main page check box to add widget to the favorites on home page (optional).

  4. Click Save to create the widget.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.